Re: i.MX6ULL Watchdog

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Re: i.MX6ULL Watchdog

2,903 次查看
bimal
Contributor III

Hi,

Thanks for reply,

I have referred to EVK boards, but i don't want to use inbetween Voltage supervisor IC.

Instead of this i want to give the WDOG_Any pin to nPOR input of i.mx6ULL processor.

Here my concern is whether POR will be able to detect the pulse of WDOG_Any pin?

Also i would like to get info that whether the internal Software reset signal will restart i.mx6ull processor(which is generated after watchdog timer expires) ?

0 项奖励
回复
1 回复

552 次查看
Yuri
NXP Employee
NXP Employee

Hello,


  It is highly recommended to remove power (voltage source) of all

components on the board in the event of a processor reset in order

to avoid i.MX SoC boot issues when power not removed during reset.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复