Hello,
You may use Table 5-9 (Fusemap Descriptions) of the i.MX6UL RM.
Column Fuse Address = 460 corresponds bank 0, word 6 in U-boot.
Value 0x00000010 means BT_FUSE_SEL is set; it means fuse only boot,
no ability for GPIO based boot configuration.
BOOT_MODE[1,0]=00 is used for boot from fuses, but boot fuses will be always
used, if BT_FUSE_SEL=1
For testing different fuse configurations BT_FUSE_SEL may be leave in default non-burned
state. If You want to apply the fuses as boot configuration finally, after debugging finish, it is
needed to burn BT_FUSE_SEL.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------