Re: PMIC PF3000 RESETBMCU signal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Re: PMIC PF3000 RESETBMCU signal

ソリューションへジャンプ
491件の閲覧回数
marklu
Contributor II

Hi Igor,

Thanks for your quick reply.

Do you know why it set default mode instead of fault mode? It seems fault mode get better reliability, don't it?

BRs

Mark

0 件の賞賛
返信
1 解決策
411件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  You are right, the PMIC fault mode is intended for most reliable applications.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
412件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  You are right, the PMIC fault mode is intended for most reliable applications.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------