Re: PMIC PF3000 RESETBMCU signal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: PMIC PF3000 RESETBMCU signal

Jump to solution
491 Views
marklu
Contributor II

Hi Igor,

Thanks for your quick reply.

Do you know why it set default mode instead of fault mode? It seems fault mode get better reliability, don't it?

BRs

Mark

0 Kudos
Reply
1 Solution
411 Views
Yuri
NXP Employee
NXP Employee

Hello,

  You are right, the PMIC fault mode is intended for most reliable applications.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
412 Views
Yuri
NXP Employee
NXP Employee

Hello,

  You are right, the PMIC fault mode is intended for most reliable applications.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------