i.MX6UL Linux not booting on SD1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6UL Linux not booting on SD1

957 Views
PramodKumar
Contributor IV

Hi,

 

We have designed our board using i.MX6UL processor with reference of i.MX6UL EVK only difference is Botting media SD card is on SD1 channel while in EVK booting channel is SD2.

 

the booting msg of board as given below

 

U-Boot 2015.04imx_v2015.04_4.1.15_1.2.0_ga+gede7538 (Apr 22 2017 - 15:12:20)

 

CPU:   Freescale i.MX6UL rev1.2 at 396 MHz
CPU:   Temperature 31 C
Reset cause: POR
Board: MX6UL 14x14 EVK
I2C:   ready
DRAM:  512 MiB
force_idle_bus: sda=0 scl=0 sda.gp=0x1d scl.gp=0x1c
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
Using default environment

 

In:    serial                                                                   
Out:   serial                                                                   
Err:   serial                                                                   
switch to partitions #0, OK                                                     
mmc0 is current device                                                          
Net:   FEC0                                                                     
Error: FEC0 address not set.                                                    
                                                                                
Normal Boot                                                                     
Hit any key to stop autoboot:  0                                                
switch to partitions #0, OK                                                     
mmc0 is current device                                                          
switch to partitions #0, OK                                                     
mmc0 is current device                                                          
** No partition table - mmc 0 **                                                
** No partition table - mmc 0 **                                                
Booting from net ...                                                            
*** ERROR: `ethaddr' not set                                                    
*** ERROR: `ethaddr' not set     

 

 

My boards not booting ahead from above msg.

 

While same SD card booted up to linux login in i.MX6UL EVK.

 

Regards,

Pramod Kumar

Labels (1)
0 Kudos
Reply
1 Reply

734 Views
joanxie
NXP TechSupport
NXP TechSupport

need to change SW601 Bit2-Bit3 from 0-1 to 1-0, then it would boot from SD1.

0 Kudos
Reply