Hi,
We are planning to use i.MX 6ULL processor and NHD-2.8-240320AF-CSXP-FT display with in-built ST7789V controller using 16-bit interface in one of our projects. While we had searched for the device drivers for the display we hadn't able to find anything and when we asked the display vendor also they said that they are not having any Linux device drivers but they had given Arduino code for the same. When we are surfing through the internet we had found one NXP community case where they were asking the similar type of question for 6UL and 7D processor. We have followed the same procedure for 6ULL processor also and created a patch file for the same which is also attached in this case. We had changed the LCD setup as per the procedure given in the link provided by the display vendor in the mxsfb_st7789s_qvga.c file. Important HW connections for the LCD with the processor is listed below.
LCD Side Pins | Processor Side Pins |
---|---|
/CS | GND |
D/C | LCD_HSYNC |
/WR | LCD_CLK |
/RD | LCD_ENABLE |
DB0-DB15 | LCD_DATA00-LCD_DATA15 |
/RES | LCD_RESET |
IM0 | GND |
We wish to know that whether the changes done by us in kernel source is correct or not and is there any further changes needed to be done in U-boot?
Thanks in advance,
Ranjith
Hi Igor,
Thanks for your quick reply. The links what you have provided uses SPI interface between processor and LCD but in our case the interface we will be using is 8080 MPU interface with bus-width as 16 and it has been given in the LCD datasheet and I also given pin mapping between LCD and processor. So it will be helpful for us if there are references using the above said interface.
Regards,
Ranjith
Hi Ranjith
for mpu one can look at patch
Patch to support MPU 8080 LCD on iMX6UL and iMX7D
Best regards
igor
Hi Igor,
Yes I had created the patch file which I had attached earlier by taking reference from that link only. My query is like it was given for 6UL and 7D and that too for a different controller so I need to know whether the patch which I had attached is correct or not and is there any further modifications need to be done in kernel and u-boot source code with 6ULL processor and the display which I had specified?
Regards,
Ranjith
Hi,
Also I have found another driver for the controller called fb_st7789v.c in drivers/staging/fbtft folder. So for what will this driver be used for and whether can we use this driver for our case?
Regards,
Ranjith
Hi Ranjith
nxp has special service for helping with porting drivers and
reviewing customers codes: Commercial Support and Engineering Services | NXP
Best regards
igor
Hi Ranjith
one can check similar case on
https://community.nxp.com/thread/451152
ST7789V driver can be found on
linux/panel-sitronix-st7789v.c at master · torvalds/linux · GitHub
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------