Qt applications are not proprely working (huge delay) on i.MX6UL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Qt applications are not proprely working (huge delay) on i.MX6UL

跳至解决方案
1,390 次查看
Poornesh7
Contributor II

We are using i.MX6UL SoC for our project . We have successfully integrated LCD to our custom carrier board and we have successfully built yocto images (Yocto : Zeus ,DISTRO=fsl-imx-wayland )for the target SoC .

But when I try to run Qt application it is very slow and I could not able to do any functionalities .

So requesting to kindly suggest me whether I need to add any Qt related packages or need to build again for any other DISTRO .

Thanks in advance

0 项奖励
回复
1 解答
1,369 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

You should use fsl-imx-fb to build, i.MX6UL only supports Frame Buffer graphics.

在原帖中查看解决方案

2 回复数
1,370 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

You should use fsl-imx-fb to build, i.MX6UL only supports Frame Buffer graphics.

1,355 次查看
Poornesh7
Contributor II

Thanks for your valuable response !

It's gald to inform you that our Qt application is working as expected without any delay after building with "fsl-imx-fb" as mentioned.

But I have other query , we have developed our Qt application with some animations (gifs) . But here these animations are not running .

Please kindly suggest me whether I need to add any extra packages for animations (gifs) to run . 

0 项奖励
回复