But an image is already present in the SD Card........... All those processes have been done and the SD Card has been give to me loaded.....
Board: MX51 BABBAGE 3.0 [POR]
Boot Device: SPI NOR
I2C: ready
DRAM: 512 MB
MMC: FSL_ESDHC: 0, FSL_ESDHC: 1
*** Warning - bad CRC or MMC, using default environment
In: serial
Out: serial
Err: serial
PMIC Mode: SPI
Net: got MAC address from IIM: 00:04:9.........
FEC0 [PRIME]
Hit any key to stop autoboot: 0
*** ERROR: `serverip' not set
Wrong Image Format for bootm command
ERROR: can't get kernel image!
This is the complete error code
Quite simple, set the serverip variable in uboot :-)
When fetching kernel image using TFTP, you need to have serverip value set so that uboot know where to fetch the kernel from.