After starting wpa_supplicant and running "wpa_cli", except typing "status", other commands return "UNKNOWN COMMAND", please kindly advise.
root@sabresd_6dq:/system/lib/modules # insmod cfg80211.ko
cfg80211: Calling CRDA to update world regulatory domain
ath=/system/etc/firmware/nvram.txt iface_name=wlan0" <
dhd_module_init: Enter
======== PULL WL_REG_ON HIGH! ========
=========== WLAN placed in POWER ON ========
bcmsdh_register: Linux Kernel SDIO/MMC Driver
dhd_conf_set_hw_oob_intr: Enable HW OOB for 43362
F1 signature OK, socitype:0x1 chip:0xa962 rev:0x1 pkg:0x9
DHD: dongle ram size is set to 245760(orig 245760) at 0x0
dhdsdio_probe: Disable prop_txstatus
dhd_conf_set_fw_name_by_chip: firmware_path=/system/etc/firmware/fw_bcm40181a2.bin
wl_create_event_handler(): thread:wl_event_handler:3a8 started
tsk Enter, tsk = 0x98401444
dhd_attach(): thread:dhd_watchdog_thread:3a9 started
dhd_attach(): thread:dhd_dpc:3aa started
dhd_attach(): thread:dhd_sysioc:3ab started
Broadcom Dongle Host Driver: register interface [wlan0] MAC: 00:90:4c:11:22:33
Dongle Host Driver, version 1.88.45.4 (r420671)
Compiled in drivers/net/wireless/bcmdhd on Sep 11 2015 at 16:12:53
======== PULL WL_REG_ON LOW! (flag = 2) ========
=========== WLAN placed in RESET ========
dhd_module_init: Exit error=0
root@sabresd_6dq:/system/lib/modules # ifconfig wlan0 up
dhd_open: Enter bcbd6000
dhd_conf_set_fw_name_by_chip: firmware_path=/system/etc/firmware/fw_bcm40181a2.bin
Dongle Host Driver, version 1.88.45.4 (r420671)
Compiled in drivers/net/wireless/bcmdhd on Sep 11 2015 at 16:12:53
wl_android_wifi_on in 1
wl_android_wifi_on in 2: g_wifi_on=0
======== PULL WL_REG_ON HIGH! (flag = 2) ========
=========== WLAN going back to live ========
sdio_reset_comm():
sdio_read_cis: 2 callbacks suppressed
mmc1: queuing unknown CIS tuple 0x80 (2 bytes)
mmc1: queuing unknown CIS tuple 0x80 (3 bytes)
mmc1: queuing unknown CIS tuple 0x80 (3 bytes)
mmc1: queuing unknown CIS tuple 0x80 (7 bytes)
dhd_bus_devreset: == WLAN ON ==
dhd_bus_devreset called when dongle is not in reset
Will call dhd_bus_start instead
dhd_conf_set_hw_oob_intr: Enable HW OOB for 43362
dhd_conf_set_fw_name_by_chip: firmware_path=/system/etc/firmware/fw_bcm40181a2.bin
dhd_conf_read_config: Ignore config file /system/etc/firmware/config.txt
Final fw_path=/system/etc/firmware/fw_bcm40181a2.bin
Final nv_path=/system/etc/firmware/nvram.txt
Final conf_path=/system/etc/firmware/config.txt
NVRAM version: AP6181_NVRAM_V1.1_01152013
dhdsdio_write_vars: Download, Upload and compare of NVRAM succeeded.
dhd_bus_init: delay 100ms for BCM43362
dhd_bus_init: enable 0x06, ready 0x06 (waited 0us)
bcmsdh_set_drvdata: Enter
bcmsdh_register_oob_intr: Enter
bcmsdh_register_oob_intr: IRQ=336 Type=414
dhd_conf_set_band: Set band 0
Firmware up: op_mode=0x0005, Broadcom Dongle Host Driver mac=98:3b:16:dd:aa:88
dhd_conf_set_country: Set country ALL, revision 0
Country code: ALL (ALL/0)
dhd_conf_set_roam: Set roam_off 1
dhd_preinit_ioctls buf_key_b4_m4 set failed -23
Firmware version = wl0: Dec 10 2012 15:10:32 version 5.90.195.89.1_edon/off_0xb8bf FWID 01-ff
Driver: 1.88.45.4 (r420671)
Firmware: wl0: Dec 10 2012 15:10:32 version 5.90.195.89.1_edon/off_0xb8bf FWID 01-ff
wl_android_wifi_on: Success
dhd_open: Exit ret=0
root@sabresd_6dq:/system/lib/modules # start wpa_supplicant
root@sabresd_6dq:/system/lib/modules # Connectting with 00:19:be:30:4b:a7 channel (6) ssid "asguest", len (7)
wl_bss_connect_done succeeded with 00:19:be:30:4b:a7
wl_notify_connect_status nothing
wl_bss_connect_done succeeded with 00:19:be:30:4b:a7
nf_conntrack: automatic helper assignment is deprecated and it will be removed soon. Use the iptables CT target to attach helpers instead.
root@sabresd_6dq:/system/lib/modules # wpa_cli
wpa_cli v2.1-devel-4.4.3
Copyright (c) 2004-2013, Jouni Malinen <j@w1.fi> and contributors
This software may be distributed under the terms of the BSD license.
See README for more details.
Using interface 'wlan0'
Interactive mode
> status
p2p_device_address=98:3b:16:dd:aa:88
p2p_state=IDLE
wifi_display=1
ifname=wlan0
address=98:3b:16:dd:aa:88
> scan
UNKNOWN COMMAND
> ifname
UNKNOWN COMMAND
>
what did u dhd_wlan_set_carddetect look like?
what does u dts file for sdio wifi look like?
Hi Jackie Chau,
About the wifi BCM43362 porting you can refer to the follow document:
Hope this can help you.
Have a nice day
Best Regards
Dan
Hello Jackie,
Give you some suggestions, see messages below :
(1) check your wpa_supplicant.conf file.
ctrl_interface=wlan0( or for unix mode: =DIR/data/misc/wifi/wpa_supplicant GROUPU=WIFI)
ap_scan=1
update_config=1
(2)wpa_cli command like this:
#wpa_cli -i wlan0
>scan
>ok
Except above, the following is my additional advice, you can also try, if you still have question, you can search "wireless-tools" on internet to get more information about debugging wireless net :
(1) Pay attention to checking the settings of router
(2)Using iwconfig to configure router
such as:
#iwconfig wlan0 mode Managed
#iwconfig wlan0 key 1234567890 (note: should be the password of your router)
#iwconfig wlan0 key open
#iwconfig wlan0 essid TP-LINK_432F1 ( note: router's name)
(3)Getting dynamic IP
# /system/bin/dhcpcd wlan0
(4)Searching AP
you can also use iwlist command to search AP, like this:
# iwlist wlan0 scan
Regards,
Weidong
Hi Weidong,
Thanks for your reply. It seems wifi module can get a dynamic IP by command line. Please take a look on the debug message. However when I move the slide switch from off to on in GUI wifi setting of Android, I can't see any debug message related to insmod *.ko or start wpa_supplicant, in logcat I just see "D/WifiService( 450): setWifiEnabled: true pid=705, uid=1000". I have followed vendor's suggestion to modify *.mk as below. Please kindly advise.
Debug message to open wifi by command line
root@sabresd_6dq:/ #
insmod /system/lib/modules/bcmdhd.ko "firmware_path=/system/etc/firmware/fw_bcm40181a2.bin nvram_path=/system/etc/firmware/nvram.txt iface_name=wlan0"
dhd_module_init: Enter
======== PULL WL_REG_ON HIGH! ========
=========== WLAN placed in POWER ON ========
bcmsdh_register: Linux Kernel SDIO/MMC Driver
dhd_conf_set_hw_oob_intr: Enable HW OOB for 43362
F1 signature OK, socitype:0x1 chip:0xa962 rev:0x1 pkg:0x9
DHD: dongle ram size is set to 245760(orig 245760) at 0x0
dhdsdio_probe: Disable prop_txstatus
dhd_conf_set_fw_name_by_chip: firmware_path=/system/etc/firmware/fw_bcm40181a2.bin
wl_create_event_handler(): thread:wl_event_handler:3a1 started
tsk Enter, tsk = 0x98381444
dhd_attach(): thread:dhd_watchdog_thread:3a2 started
dhd_attach(): thread:dhd_dpc:3a3 started
dhd_attach(): thread:dhd_sysioc:3a4 started
Broadcom Dongle Host Driver: register interface [wlan0] MAC: 00:90:4c:11:22:33
Dongle Host Driver, version 1.88.45.4 (r420671)
Compiled in drivers/net/wireless/bcmdhd on Sep 14 2015 at 10:23:19
======== PULL WL_REG_ON LOW! (flag = 2) ========
=========== WLAN placed in RESET ========
dhd_module_init: Exit error=0
root@sabresd_6dq:/ # ifconfig wlan0 up
dhd_open: Enter bc946800
dhd_conf_set_fw_name_by_chip: firmware_path=/system/etc/firmware/fw_bcm40181a2.bin
Dongle Host Driver, version 1.88.45.4 (r420671)
Compiled in drivers/net/wireless/bcmdhd on Sep 14 2015 at 10:23:19
wl_android_wifi_on in 1
wl_android_wifi_on in 2: g_wifi_on=0
======== PULL WL_REG_ON HIGH! (flag = 2) ========
=========== WLAN going back to live ========
sdio_reset_comm():
mmc1: queuing unknown CIS tuple 0x80 (2 bytes)
mmc1: queuing unknown CIS tuple 0x80 (3 bytes)
mmc1: queuing unknown CIS tuple 0x80 (3 bytes)
mmc1: queuing unknown CIS tuple 0x80 (7 bytes)
dhd_bus_devreset: == WLAN ON ==
dhd_bus_devreset called when dongle is not in reset
Will call dhd_bus_start instead
dhd_conf_set_hw_oob_intr: Enable HW OOB for 43362
dhd_conf_set_fw_name_by_chip: firmware_path=/system/etc/firmware/fw_bcm40181a2.bin
dhd_conf_read_config: Ignore config file /system/etc/firmware/config.txt
Final fw_path=/system/etc/firmware/fw_bcm40181a2.bin
Final nv_path=/system/etc/firmware/nvram.txt
Final conf_path=/system/etc/firmware/config.txt
NVRAM version: AP6181_NVRAM_V1.1_01152013
dhdsdio_write_vars: Download, Upload and compare of NVRAM succeeded.
dhd_bus_init: delay 100ms for BCM43362
dhd_bus_init: enable 0x06, ready 0x06 (waited 0us)
bcmsdh_set_drvdata: Enter
bcmsdh_register_oob_intr: Enter
bcmsdh_register_oob_intr: IRQ=336 Type=414
dhd_conf_set_band: Set band 0
Firmware up: op_mode=0x0005, Broadcom Dongle Host Driver mac=98:3b:16:dd:aa:88
dhd_conf_set_country: Set country ALL, revision 0
Country code: ALL (ALL/0)
dhd_conf_set_roam: Set roam_off 1
dhd_preinit_ioctls buf_key_b4_m4 set failed -23
Firmware version = wl0: Dec 10 2012 15:10:32 version 5.90.195.89.1_edon/off_0xb8bf FWID 01-943eb0bc
Driver: 1.88.45.4 (r420671)
Firmware: wl0: Dec 10 2012 15:10:32 version 5.90.195.89.1_edon/off_0xb8bf FWID 01-943eb0bc
wl_android_wifi_on: Success
dhd_open: Exit ret=0
root@sabresd_6dq:/ # start wpa_supplicant
root@sabresd_6dq:/ # Connectting with 00:19:be:30:4b:a7 channel (6) ssid "asguest", len (7)
wl_bss_connect_done succeeded with 00:19:be:30:4b:a7
wl_notify_connect_status nothing
wl_bss_connect_done succeeded with 00:19:be:30:4b:a7
nf_conntrack: automatic helper assignment is deprecated and it will be removed soon. Use the iptables CT target to attach helpers instead.
root@sabresd_6dq:/ # dhcpcd wlan0
dhcpcd[960]: version 5.5.6 starting
dhcpcd[960]: wlan0: checking for 169.254.251.58
dhcpcd[960]: wlan0: using IPv4LL address 169.254.251.58
dhcpcd[960]: forked to background, child pid 985
logcat to open wifi via GUI
W/AudioTrack( 444): AUDIO_OUTPUT_FLAG_FAST denied by client due to mismatching sample rate (48000 vs 44100)
I/ActivityManager( 444): START u0 {act=android.intent.action.MAIN cmp=com.android.settings/.SubSettings (has extras)} from pid 695
D/SubSettings( 695): Launching fragment com.android.settings.wifi.WifiSettings
E/BufferQueue( 143): [com.android.settings/com.android.settings.SubSettings] dequeueBuffer: can't dequeue multiple buffers without setting the buffer count
I/ActivityManager( 444): Displayed com.android.settings/.SubSettings: +204ms
D/WifiService( 444): setWifiEnabled: true pid=695, uid=1000
W/SocketClient( 141): write error (Broken pipe)
D/ConnectivityService( 444): Sampling interval elapsed, updating statistics ..
D/ConnectivityService( 444): Done.
D/ConnectivityService( 444): Setting timer for 720seconds
I/MediaFocusControl( 444): AudioFocus abandonAudioFocus() from android.media.AudioManager@2c891d18com.android.music.MediaPlaybackService$3@2c890b98
I/ActivityManager( 444): Start proc com.android.musicfx for broadcast com.android.musicfx/.ControlPanelReceiver: pid=962 uid=10010 gids={50010, 3003, 3002}
V/MusicFXControlPanelReceiver( 962): onReceive
V/MusicFXControlPanelReceiver( 962): Action: android.media.action.CLOSE_AUDIO_EFFECT_CONTROL_SESSION
V/MusicFXControlPanelReceiver( 962): Package name: com.android.music
V/MusicFXControlPanelReceiver( 962): Audio session: 7
V/MusicFXControlPanelEffect( 962): closeSession(android.app.ReceiverRestrictedContext@2c88d000, com.android.music, 7)
In BoardConfig.mk,
BOARD_WPA_SUPPLICANT_DRIVER := NL80211
WPA_SUPPLICANT_VERSION := VER_0_8_X
BOARD_WPA_SUPPLICANT_PRIVATE_LIB := lib_driver_cmd_bcmdhd
BOARD_HOSTAPD_DRIVER := NL80211
BOARD_HOSTAPD_PRIVATE_LIB := lib_driver_cmd_bcmdhd
BOARD_WLAN_DEVICE := bcmdhd
WIFI_DRIVER_FW_PATH_PARAM := "/sys/module/bcmdhd/parameters/firmware_path"
WIFI_DRIVER_FW_PATH_STA := "/system/etc/firmware/fw_bcm40181a2.bin"
WIFI_DRIVER_FW_PATH_P2P := "/system/etc/firmware/fw_bcmbcm40181a2_p2p.bin"
WIFI_DRIVER_FW_PATH_AP := "/system/etc/firmware/fw_bcmbcm40181a2_apsta.bin"
WIFI_DRIVER_MODULE_NAME := "bcmdhd"
#WIFI_DRIVER_MODULE_PATH := "/system/lib/modules/bcmdhd.ko"
WIFI_DRIVER_MODULE_ARG := "iface_name=wlan0 firmware_path=/system/etc/firmware/fw_bcmbcm40181a2.bin nvram_path=/system/etc/firmware/nvram.txt"
In android/external/wpa_supplicant_8/wpa_supplicant/wpa_supplicant.conf
update_config=1
ctrl_interface=wlan0
eapol_version=1
ap_scan=1
fast_reauth=1
In init.rc
on post-fs-data
mkdir /data/misc/wifi 0770 wifi wifi
mkdir /data/misc/wifi/sockets 0770 wifi wifi
mkdir /data/misc/dhcp 0770 dhcp dhcp
on boot
service wpa_supplicant /system/bin/wpa_supplicant \
-iwlan0 -Dnl80211 -c/data/misc/wifi/wpa_supplicant.conf \
-I/system/etc/wifi/wpa_supplicant_overlay.conf \
-O/data/misc/wifi/sockets \
-e/data/misc/wifi/entropy.bin -g@android:wpa_wlan0
class main
socket wpa_wlan0 dgram 660 wifi wifi
disabled
oneshot
service p2p_supplicant /system/bin/wpa_supplicant \
-iwlan0 -Dnl80211 -c/data/misc/wifi/p2p_supplicant.conf \
-I/system/etc/wifi/p2p_supplicant_overlay.conf -N \
-O/data/misc/wifi/sockets \
-e/data/misc/wifi/entropy.bin -g@android:wpa_wlan0 \
-puse_p2p_group_interface=1p2p_device=1
class main
socket wpa_wlan0 dgram 660 wifi wifi
disabled
oneshot
service dhcpcd_wlan0 /system/bin/dhcpcd -ABKL
class main
disabled
oneshot
service dhcpcd_p2p /system/bin/dhcpcd -aABKL
class main
disabled
oneshot
service iprenew_wlan0 /system/bin/dhcpcd -n
class main
disabled
oneshot
service iprenew_p2p /system/bin/dhcpcd -n
class main
disabled
oneshot