PN7150 TListen time tuning in android 11

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7150 TListen time tuning in android 11

548 Views
TNK
Contributor I

Hi,

In our current project we using IMX8MM with NXP's own PN7150 NFC which runs Android 11. We have successfully integrated and have a working solution on the custom board, BUT we wanted to decrease to TListen time from 550 Ms which we are currently observing down to 250 or 300 ms.

from all the documents we found 

Name               NCI Tag  Length Default value     Description

Total_Duration 0x00               2    0xE803            Total duration of the single discovery period in [ms-Little endian coded] TLISTEN = Total_Duration - TPOLL

 



reference: AN11757.pdf


We tried to add the same to libnxp-nfc.conf 

# Core configuration settings
NXP_CORE_CONF={ 20, 02, 2B, 0D,

00, 2C, 01
28, 01, 00,
21, 01, 00,
30, 01, 08,
31, 01, 03,
33, 04, 01, 02, 03, 04,
54, 01, 06,
50, 01, 02,
5B, 01, 00,
60, 01, 0E,
80, 01, 01,
81, 01, 01,
82, 01, 0E,
18, 01, 01
}

But we have not observed any change in TListen times on the oscilloscope.

 

 

Thank you

 

0 Kudos
Reply
0 Replies