PMIC that support Li-ion battery charging and fuel gauge for i.MX 8M Quad

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PMIC that support Li-ion battery charging and fuel gauge for i.MX 8M Quad

Jump to solution
1,222 Views
andy_kim
Contributor IV

Hello,

 

The recommended PMIC is PF4210 for i.MX 8M Quad.

And PF4210 is applied to MCIMX8M-EVK for i.MX 8M Quad.

 

However, when I checked the battery charging function. it has only coin-cell charger on PF4210.

Are there any NXP PMIC solution that support Li-ion battery charging and Fuel gauge with i.MX 8M Quad?

And How to do battery profile simulation for fuel gauge accuracy? Is there a simulation tool for customer to do battery profiling? 

 

Thank you,

Andy

 

Labels (1)
0 Kudos
Reply
1 Solution
1,209 Views
igorpadykov
NXP Employee
NXP Employee
4 Replies
1,219 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andy

 

I am afraid such pmic is not available, sorry. In general one can try to use external charger chip.

 

Best regards
igor

0 Kudos
Reply
1,211 Views
andy_kim
Contributor IV

Dear igor,

Thanks for your prompt feedback.

If it is available, Can you recommend for me any external charger chip that have been used for the application?

 

Thanks,

Andy

0 Kudos
Reply
1,210 Views
igorpadykov
NXP Employee
NXP Employee

for example one can look at Sabre SD schematic spf-27392 p.18

 

Design files, including hardware schematics, Gerbers, and OrCAD files for i.MX 6Quad (i.MX 6Dual emu...

 

Best regards
igor

1,204 Views
andy_kim
Contributor IV

Dear igor

Thanks for your support.

0 Kudos
Reply