Hi,
I am trying to figure out the first power up of the imX6ULL.
I am planning to power the SNVS with a 3.3V LDO and provide the PMIC_ON_REQ as the enable signals for the switchers providing 3v3 and 1v8 voltages.
1) will the PMIC_ON_REQ (pin T9 be) automatically asserted on powering up the VSS_SNVS_IN?
Thanks and Regards
Amal A G
Solved! Go to Solution.
Hi @AMAL-DICORTECH,
I hope you are doing well.
Since there is an internal Pull up (100K) of VDD_SNSVS_IN power rail on the PMIC_ON_REQ pin, as soon as the SNVS voltage is turned ON, the PMIC_ON_REQ pin will be driven high.
Please make sure to follow the power-up sequence mentioned in the datasheet. For reference, one can refer to the iMX6ULL EVK schematic design.
Thanks & Regards,
Ritesh M Patel
Hi, @riteshmpatel,
I am having another query regarding the PMIC_ON_REQ pin in i.MX6.ULL. Can you please comment on the amount of current that can be sourced from this pin .
Hi @AMAL-DICORTECH,
I hope you are doing well.
Since there is an internal Pull up (100K) of VDD_SNSVS_IN power rail on the PMIC_ON_REQ pin, as soon as the SNVS voltage is turned ON, the PMIC_ON_REQ pin will be driven high.
Please make sure to follow the power-up sequence mentioned in the datasheet. For reference, one can refer to the iMX6ULL EVK schematic design.
Thanks & Regards,
Ritesh M Patel