Hi all
I want to know whether PMIC_ON_REQ is open drain or not.
I would like to control PWRON of PMIC in two ways from another device.
One is PMIC_ON_REQ and the other is other external device.
According to the SDB schematic, PWRON is connected with PMIC_ON_REQ and PMIC_PWRON.
I think the PMIC_PWRON is Open drain so there is no problem.
However, there is no description that whether PMIC_ON_REQ is Open drain or not.
Is the PMIC_ON_REQ also Open drain ?
If yes, please let me know where I can find the description.
Ko-hey
Solved! Go to Solution.
Hi Ko-hey
yes it is open-drain please refer to part of datasheet
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Ko-hey
yes it is open-drain please refer to part of datasheet
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I have a similar question regarding the PMIC_ON_REQ configuration on the i.MX7D Sabre board.
It seems to be the same (PMIC PWRON is driven by both i.MX7D PMIC_ON_REQ as well as an open-drain PMIC_PWRON signal from a supervisor IC).
Is the PMIC_ON_REQ on the i.MX7D also open-drain? I ask, because it is not specified in the datasheet, and in the hardware development guide for the i.MX7D it says that PMIC_ON_REQ is a push-pull output:
If this is true, then whenever the supervisor IC pulls PMIC_PWRON low, it would be in contention with the i.MX7D push-pull output. Can you please clarify this?
@otsl
Hello,
the issue was already discussed in
https://community.nxp.com/t5/i-MX-Processors/about-PMIC-ON-REQ-pin-on-i-MX7-Dual/m-p/1153390
Regards,
Yuri.
Hi Igor
The datasheet which you showed is for i.MX6D/Q. But I use i.MX6SoloX.
Is it same as i.MX6SoloX ?
Ko-hey
Hi Ko-hey
yes. i.MX6SoloX was developed from i.MX6Solo.
Best regards
igor
Hi Igor
Thanks.
Can I request the description to NXP by TIC ?
Ko-hey
Hi Ko-hey
if you have special reasons, please escalate this through local fae channel.
Note you will have to submit customer project info and (probably)
have valid NDA with nxp.
Best regards
igor
Hi Igor
Thanks you !
Ko-hey