Hi I need help capturing MP4 videos using openCV and GSTREAMER.
Environment:
Board: i.MX8 Quad Max MEK
Linux: NXP i.MX Release Distro 5.4-zeus imx8qmmek
This is the way I'm playing back MP4 the videos:
gst-launch-1.0 filesrc location=/home/LH.mp4 ! video/quicktime ! aiurdemux ! queue ! h264parse ! v4l2h264dec ! imxvideoconvert_g2d ! queue ! waylandsink
So based on that I built the following pipeline for VideoCapture function:
cv::VideoCapture LHcap("filesrc location=/home/LH.mp4 ! video/quicktime ! aiurdemux ! queue ! h264parse ! v4l2h264dec ! imxvideoconvert_g2d ! queue ! appsink", cv::CAP_GSTREAMER)
But, the frames captured has only 2 channel and all OpenCV conversion functions fails.
cv::Mat img;
LHcap >> img;
cout << img.channels() << endl;
So i tried another pipeline
filesrc location=/home/LH.mp4 ! decodebin ! videorate ! video/x-raw,framerate=1/1 ! videoconvert ! video/x-raw, format=(string)BGR ! appsink
using this pipeline, the captured images have 3 channels and the type is well recognized (CV_8UC3), BUT, if I save one of the frames, I can see the image is broken
(See attached)
Does anybody knows how to capture mp4 videos using opencv and GSREAMER?
Thanks
Seba.-
Solved! Go to Solution.
I was able to make it work..
const std::string pipeline = "filesrc location=/home/videos/RH-yuv420-slow.mp4 ! video/quicktime ! aiurdemux ! queue ! h264parse ! v4l2h264dec ! imxvideoconvert_g2d ! capsfilter caps=\"video/x-raw,format=UYVY,width=1392,height=512\" ! videoconvert ! queue ! appsink";
cv::VideoCapture cap(pipeline, cv::CAP_GSTREAMER);
const int camID = 3;
cv::VideoCapture CAMcap(camID, cv::CAP_GSTREAMER);
I was able to make it work..
const std::string pipeline = "filesrc location=/home/videos/RH-yuv420-slow.mp4 ! video/quicktime ! aiurdemux ! queue ! h264parse ! v4l2h264dec ! imxvideoconvert_g2d ! capsfilter caps=\"video/x-raw,format=UYVY,width=1392,height=512\" ! videoconvert ! queue ! appsink";
cv::VideoCapture cap(pipeline, cv::CAP_GSTREAMER);
const int camID = 3;
cv::VideoCapture CAMcap(camID, cv::CAP_GSTREAMER);