Hi,
I am new to NXP. I am using Evaluation Kit SABRE similar to SABRE|Automotive-Infotainment|i.MX6 | NXP Semiconductors which is having MCIMX6U6AVM08AB DualLite processor [800Mhz].
I have prepared the build for it using
DISTRO=fsl-imx-wayland MACHINE=imx6dlsabresd source imx-setup-release.sh -b ../build
Then I have written wic image using
sudo dd if=core-image-minimal-imx6dlsabresd.wic of=dev/sdb bs=4096 && sync
Then I tried to boot it. But it is not booting.
I have followed the same steps for other machine imx6qdlsabreauto in corresponding EV kit. It is booted fine. Could anyone can help me? Any jumper/boot switch issue in board or any bootloader mismatch issue/DDR failure?
解決済! 解決策の投稿を見る。
Hi,
I have downloaded LF_v5.10.72-2.2.3_images_IMX6QPDLSOLOX BSP.
From there I have taken u-boot-imx6dlsabreauto_sd.imx and flashed it using
"sudo uuu -b sd u-boot-imx6dlsabreauto_sd.imx".
Now I can see the logs from console. Now it is booting fine.
U-Boot 2021.04-lf_v2021.04+g8b8a0e5567 (Sep 27 2022 - 02:05:23 +0000)
CPU: i.MX6DL rev1.1 at 792MHz
CPU: Automotive temperature grade (-40C to 125C) at 55C
Reset cause: POR
Model: i.MX6 DualLite/Solo SABRE Automotive Board
Board: MX6Q-Sabreauto revO
DRAM: 2 GiB
PMIC: PFUZE100! DEV_ID=0x10 REV_ID=0x11
MMC: FSL_SDHC: 0, FSL_SDHC: 2
Loading Environment from MMC... *** Warning - bad CRC, using default environment
No panel detected: default to Hannstar-XGA
Now, we have build system for imx-yocto-bsp. Tried to build for machine name "imx6dlsabreauto" which I modified in local.conf . But I faced error as invalid machine name when do bitbake. Kindly refer the attached image "invalid_machine". Then I looked for conf in source folders, I can't find conf file for imx6dlsabreauto . Kindly refer the attached image "CONF_files". Is that deprecated/removal of support for this machine from the current linux release?
Now can you please answer to the question "what is the machine name that should I used for build the image for EVK NXP board MCIMXABASEV1 which is having processor MCIMX6U6AVM08AB?"
Thanks for the understanding.
Hi,
I have downloaded LF_v5.10.72-2.2.3_images_IMX6QPDLSOLOX BSP.
From there I have taken u-boot-imx6dlsabreauto_sd.imx and flashed it using
"sudo uuu -b sd u-boot-imx6dlsabreauto_sd.imx".
Now I can see the logs from console. Now it is booting fine.
U-Boot 2021.04-lf_v2021.04+g8b8a0e5567 (Sep 27 2022 - 02:05:23 +0000)
CPU: i.MX6DL rev1.1 at 792MHz
CPU: Automotive temperature grade (-40C to 125C) at 55C
Reset cause: POR
Model: i.MX6 DualLite/Solo SABRE Automotive Board
Board: MX6Q-Sabreauto revO
DRAM: 2 GiB
PMIC: PFUZE100! DEV_ID=0x10 REV_ID=0x11
MMC: FSL_SDHC: 0, FSL_SDHC: 2
Loading Environment from MMC... *** Warning - bad CRC, using default environment
No panel detected: default to Hannstar-XGA
Now, we have build system for imx-yocto-bsp. Tried to build for machine name "imx6dlsabreauto" which I modified in local.conf . But I faced error as invalid machine name when do bitbake. Kindly refer the attached image "invalid_machine". Then I looked for conf in source folders, I can't find conf file for imx6dlsabreauto . Kindly refer the attached image "CONF_files". Is that deprecated/removal of support for this machine from the current linux release?
Now can you please answer to the question "what is the machine name that should I used for build the image for EVK NXP board MCIMXABASEV1 which is having processor MCIMX6U6AVM08AB?"
Thanks for the understanding.
It is imx6qdlsabreauto
Hi,
Can anyone help on below question?
Hi,
I am using nxp reference board.
S2:
1-OFF.
2-OFF.
3-ON.
4.OFF.
S1:
1-OFF
2-ON
3-OFF
4-OFF
5-ON
6-ON
7-OFF
8-OFF
9-OFF
10-OFF
S3: (BOOT MODE)
1-ON
2-ON
3-OFF
4-OFF
Are you using the NXP reference board or the third company board? If it is nxp board have you set the proper boot up mode for it?