I am using a imx6 based custom board
Made the build system ready using the following guide: https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf
After cloning the yocto source, initialized the build with: DISTRO=fsl-imx-fb MACHINE=imx6dlsabresd source imx-setup-release.sh -b build_imx
Then started the build using: bitbake -k core-image-minimal.
The core-image-minimal-xxxx-xxx.tar is generated. But when the board is booted with this RFS image, it did not accept any password for the root user.
I checked the local.conf. It has:
EXTRA_IMAGE_FEATURES ?= "debug-tweaks"
Yet it did not accept a blank password or any other password.
I had a look at /etc/shadow file. The root user's password field is empty.
I tried to change the password manually in /etc/shadow file, but it did not work out.
Can any one point out what should i do to fix the login issue.
已解决! 转到解答。
the root cause of the issue is:
sysvinit version that comes with the RFS image: Sysvinit version 3.01 does not allow root login through NFS boot. But sysvinit version 2.88 works fine with the existing NFS boot settings.
So I started working on the nfsboot parameters, and found that two new nfs parameters had to be added: no_root_squash,insecure
the root cause of the issue is:
sysvinit version that comes with the RFS image: Sysvinit version 3.01 does not allow root login through NFS boot. But sysvinit version 2.88 works fine with the existing NFS boot settings.
So I started working on the nfsboot parameters, and found that two new nfs parameters had to be added: no_root_squash,insecure
Hi
Thanks for the reply,
I am booting the board through NFS. So what I did is that I mounted the partition in core-image-minimal-xxxx-xxx.wic through:
1) losetup -o 33554432 /dev/loop1 core-image-minimal-imx6dlsabresd-20230110062552.rootfs.wic
2) mount /dev/loop1 /mnt/
3) copied the contents of the /mnt/ folder to my NFS folder. After booting my board and tried to login I see the "Login incorrect" message for user: root and password: root.
Note: I have changed the default systemd to sysvinit in "meta-imx/meta-sdk/conf/distro/include/fsl-imx-preferred-env.inc" will that cause any problems?
1) refer to the link https://docs.yoctoproject.org/ref-manual/classes.html#extrausers-bbclass
2)remove debug-weaks in the local.conf
This is a reference local.conf change; where the debug-tweaks has been deleted and line 30-35 showing how to set root password and add user named as user1; which has sudo capability.
MACHINE ??= 'imx6ulevk'
DISTRO ?= 'fsl-imx-fb'
PACKAGE_CLASSES ?= "package_rpm"
USER_CLASSES ?= "buildstats image-mklibs image-prelink"
PATCHRESOLVE = "noop"
BB_DISKMON_DIRS ??= "\
STOPTASKS,${TMPDIR},1G,100K \
STOPTASKS,${DL_DIR},1G,100K \
STOPTASKS,${SSTATE_DIR},1G,100K \
STOPTASKS,/tmp,100M,100K \
ABORT,${TMPDIR},100M,1K \
ABORT,${DL_DIR},100M,1K \
ABORT,${SSTATE_DIR},100M,1K \
ABORT,/tmp,10M,1K"
PACKAGECONFIG_append_pn-qemu-native = " sdl"
PACKAGECONFIG_append_pn-nativesdk-qemu = " sdl"
CONF_VERSION = "1"
DL_DIR ?= "/home/nxa15297/mydata/aosp/YoctoDN-4.9/downloads"
ACCEPT_FSL_EULA = "1"
BOOT_SPACE = "65536"
IMAGE_OVERHEAD_FACTOR = "1.5"
CORE_IMAGE_EXTRA_INSTALL += " cryptsetup cryptodev-module cryptodev-tests openssh dhcp-client dhcp-server connman"
TOOLCHAIN_HOST_TASK_append = " nativesdk-python nativesdk-python-pycrypto"
IMAGE_INSTALL_append = " sudo"
INHERIT += " extrausers"
EXTRA_USERS_PARAMS = "\
usermod -P 1876*18 root;\
useradd -P 2015*08 user1;\
usermod -a -G sudo user1;\
"
refer to the document
if you couldn't access it, pls refer to:
To set up proper sudo access for use1, bootup the system and login as root using the above root password. Then using visudo to modify the following line as:
## Uncomment to allow members of group sudo to execute any command
%sudo ALL=(ALL) NOPASSWD: ALL