Need i.MX6Q L3.0.35_4.0.0 SOURCE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need i.MX6Q L3.0.35_4.0.0 SOURCE

1,258 Views
NithinkumarN
Contributor II

Hi all,

I'm working on i.MX6Q processor.

Please let me know from where I can get L3.0.35_4.0.0 source code for i.MX6Q.

Thanks and Regards,

Nithin

Labels (1)
0 Kudos
Reply
4 Replies

1,045 Views
saurabh206
Senior Contributor III

Hi  Nithin

You can do git clone and fetch NXP kernel source code.

git clone git://git.freescale.com/imx/linux-2.6-imx.git

git checkout imx_3.0.35_4.0.0

Thanks

Saurabh

1,045 Views
zhaojunxin
Contributor I

Hi Saurabh Patel

   I have same question; Now, I am building a AVB Demo ,follow the "i.MX6 AVB Demo Implementation" wroten by xianfeng_jin , but this doc create in 2013, and all patch  is work for L3.0.35_4.0.0,  

   I do git clone and git checkout ,but cannot checkout the branch L3.0.35_4.0.0 success;

,,can you give me some help?

0 Kudos
Reply

1,045 Views
saurabh206
Senior Contributor III

Hi Zhao,

You can check git tag, there are multiple tags for different code completion.

Thanks

Saurabh

0 Kudos
Reply

1,045 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Linux BSP sources and documentation may be found on the following
Summary Page

i.MX 6 Series Software and Development Tool|NXP

In particular, below is L3.0.101_4.1.1 source package.


http://www.nxp.com/webapp/Download?colCode=L3.0.101_4.1.1_SOURCE_BSP&appType=license&location=null&P...

  If You need just L3.0.35_4.0.0 package, please enter a new request :

How to submit a new question for NXP Support

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------