NAND boot Stride Size Fuse Value

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NAND boot Stride Size Fuse Value

Jump to solution
650 Views
rickardandersso
Contributor III

The i.MX 6SoloX Applications Processor Reference Manual refers to "Stride Size Fuse Value", but I have searched the reference manual without finding the actual register. Where can I set "Stride Size Fuse Value"?

Thanks,

Rickard

Labels (1)
1 Solution
551 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The stride size is usually the pages in each block which comes from the

boot configuration (Pages In Block) : “the search area contains copies of the FCB
at each stride distance, so in case the first NAND block becomes corrupted,

the ROM will find its copy in the next NAND block.”

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

View solution in original post

1 Reply
552 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The stride size is usually the pages in each block which comes from the

boot configuration (Pages In Block) : “the search area contains copies of the FCB
at each stride distance, so in case the first NAND block becomes corrupted,

the ROM will find its copy in the next NAND block.”

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!