Mount eMMC as a disk failed in the u-boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mount eMMC as a disk failed in the u-boot

1,254 Views
Thermo_Colin
Contributor I

I have a SOM board which is  MSC SM2S-IMX8PLUS .

I tried to mount eMMC as a disk to write the new image with the command "ums 0 mmc 2", first the mount was sucessful and the disk was showed in the windows, then I write the image to the disk, but the power was shutdown unexpectedly when it's writing. After I reboot the instrument and went to the uboot console again, the command "ums 0 mmc 2" will get the result of "Couldn't find partition mmc 2".

Thermo_Colin_0-1714119220092.png

 

My understanding is the eMMC partition has been broken when image writing, but I don't know how to resolve this issue, could give me help to fix this issue? Thanks.

 

0 Kudos
Reply
1 Reply

1,217 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version BSP are you using? Can you send us your full log file to us?

0 Kudos
Reply