Hi all,
I am currently on a task to integrate the i.mx6 SOLO with WM8731. I used the imx-wm8962 as base and modified it accordingly to suit to the wm8731.
As of current progress, i had manage to link the I2C and AUDMUX between the CPU and the audio codec.
From the kernel log, i can see that the wm8731-hifi is linked with imx-ssi.0,
[ 0.484393] asoc: wm8731-hifi <-> imx-ssi.0 mapping ok
and a ALSA device is created.
[ 0.491081] ALSA device list:
[ 0.491087] #0: wm8731
In my device node, i have seen /snd/controlC0, /snd/pcmC0D0c and /snd/pcmC0D0p node.
However i do not see the /dev/audio and /dev/mixer nodes. May i know where and when does the node is created? Which part of the coding in kernel creates it? I am using kernel version 3.0.15.
Thank you
已解决! 转到解答。
Hi ZC
I would suggest to post that on alsa community as
this is specific alsa question
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thanks for the suggestion.
I would like to see if in the freescale community had anybody done the integration of wm8731 before and point me to the right direction, instead of me scratching my head thinking whether am i doing the correct thing.
I am doing the kernel space integration for the audio codec. Therefore, i need to understand where does the creation of /dev/audio and /dev/mixer take place so that i can starts my debugging and communicate with the guy who is doing the user space coding.
Thank you.