MT35XU02G cannot be used on i.MX8qxp

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MT35XU02G cannot be used on i.MX8qxp

947 次查看
george_wang
Contributor I

Hello

I am using i.MX8qxp and 4.14.98 BSP

when I use mt35xu512aba spi-nor flash, everything is fine

I can get JEDEC id through command "sf probe"

But when I use MT35XU02GCBA2G12-0AAT, there is a problem

I always get the information below

SF: unrecognized JEDEC id bytes: 00, 00, 00

How can I fix this problem

Thanks

0 项奖励
回复
1 回复

927 次查看
igorpadykov
NXP Employee
NXP Employee

Hi George

problem may be that some SPI NORs only supports octal mode even for the ReadID command. 

One can try to debug it in spi_nor_read_reg() function in driver and and make it work in octal mode:

spi-nor-core.c\spi\mtd\drivers - uboot-imx - i.MX U-Boot 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复