MMPF0100 : Is the the SWxx_PWRSTG[2:0] setting related with the ISW1ABCLIM value ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMPF0100 : Is the the SWxx_PWRSTG[2:0] setting related with the ISW1ABCLIM value ?

ソリューションへジャンプ
734件の閲覧回数
koichisakagami
Contributor II

Dear community,

We consider the MMPF0100 register setting .

The SWxx_PWRSTG[2:0] bit control the number of power stage.
Meantime, SW1A/B/C has the parameter ( ISW1ABCLIM ) "Current Limiter Peak Current Detection"

Is the SWxx_PWRSTG[2:0] bit register setting related with the ISW1ABCLIM value ?
For example, the SWxx_PWRSTG[2:0] is set to "001" (about half power),
then Does ISW1ABCLIM value decrease ?

Best Regards,
Koichi Sakagami

ラベル(1)
0 件の賞賛
返信
1 解決策
654件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi koichi

no ISW1ABCLIM does not decrease (SWxx_PWRSTG[2:0] setting not related with the ISW1ABCLIM value),

it has fixed value described in Table 53 SW1A/B/C Electrical Characteristics MMPF0100

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
655件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi koichi

no ISW1ABCLIM does not decrease (SWxx_PWRSTG[2:0] setting not related with the ISW1ABCLIM value),

it has fixed value described in Table 53 SW1A/B/C Electrical Characteristics MMPF0100

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信