Hi,
We are using i.MX8M Plus for our design. Can we modify the drive strength of Clock and Data in MIPI DSI HS mode? If yes, Is it with some property in device tree or we need to modify registers in driver?
Thank you in advance !
Regards,
Kunal
Hello NXP team,
We have verified MIPI DSI clock signal on iMX8MPlus EVK and our design (based on iMX8MPlus) , while playing 1080p videos on both interface.
Below are our observations:
---------------------------------------------
-------------------------------------------------
Please suggest if we have to change any configuration / drive strength on our custom board so that we do not violate MIPI specifications.
Thanks.
Hello NXP team,
We have reviewed our board layout with reference to i.MX 8M+ hardware developer's guide as well as NXP EVK design.
We did not find any issue (All the traces are routed differentially, solid GND plane as a reference and length-matched. Also, we verified impedance report from PCB FAB house, and all single ended / differential impedances are within 10% tolerance.)
Kindly guide us for further investigation / troubleshooting.
Thanks.
in general, support for passing compliance specifications is provided with NXP Professional Services:
https://contact.nxp.com/new-prof-svcs-sw-tech
Best regards
igor
Hi Mihir
>if we have to change any configuration / drive strength on our custom board so
>that we do not violate MIPI specifications.
this is caused by board layout (impedance mismatch) and can not be changed by software settings.
Recommended to review board layout using i.MX 8M Plus Hardware Developer’s Guide
and NXP EVK design
Best regards
igor
Hi NXP team,
This is Mihir, working with Kunal on the same design.
We are checking MIPI DSI signal levels for Design Validation Testing.
We found that, MIPI DSI Clock and Data signal levels are not compliant with MIPI D-PHY specifications v1.2. Hence, we would like to see if any register settings can be changed to reduce overall signals peak to peak value?
Thanks,
please test it on NXP i.MX8M Plus EVK reference board
Best regards
igor
Hi Kunal
mipi-dsi drive strength and output levels are defined and guaranteed by specifications
and cannot be programmed.
Best regards
igor