MIMXRT1061CVL5B QSPI flash BOOT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1061CVL5B QSPI flash BOOT

Jump to solution
605 Views
dddd
Contributor II

Hello everyone:

    Cannot execute the hello_world demo program properly. When I use jlink debug, the program stops at ResetISR(),  error info: “Break at address "0x4519fb0" with no debug information available, or outside of program code.”.

    What do I have to do to use QSPI flash boot properly?

    About our custom boards: MIMXRT1061CVL5B  + W25Q128JV

    SDK info: 581E3D70B6BE910FDB337AA8FE843242.png

    We have tried the following:

        SDK flexspi_nor_polling_transfer demo works properly. flash status register QE bit is 1.  

         qspiflash_config: 32B6F915-5A46-4429-B4F6-341268B42B56.png

    Looking forward to and thanking you for your reply.

Regards,

dddd

Labels (1)
0 Kudos
Reply
1 Solution
590 Views
dddd
Contributor II

Hi jeremyzhou,

     NXP-MCUBootUtility tool flash read and erase is ok, but board can't  boot up.

dddd_0-1652844778554.png

dddd_1-1652844819243.png

 

View solution in original post

0 Kudos
Reply
2 Replies
594 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Firstly, I'd like to suggest you use the NXP-MCUBootUtility tool to contact the board, then program an image to the QSPI and check your custom board whether can boot up successfully.
Secondly, whether you ever modify the hello_world demo when giving it debug testing.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
591 Views
dddd
Contributor II

Hi jeremyzhou,

     NXP-MCUBootUtility tool flash read and erase is ok, but board can't  boot up.

dddd_0-1652844778554.png

dddd_1-1652844819243.png

 

0 Kudos
Reply