MFG flash error on Android 7.1.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MFG flash error on Android 7.1.2

2,808件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi All,

I'm working on imx6q Android 7.1.2 platform. On by board have 4GB internal emmc. so in "device-partitions.bpt" file size i have changed to 4GB. 

{
"settings": {
"disk_size": "4 GiB",
"disk_alignment": 1048576
},

As per your procedure I followed to flash the Android images by using MFG tool. But it stopped at "Formatting cache partition" level. 

I have attached MFG logs with this post. 

Can you please provide solutions for this as soon as possible. 

Regards,

Aravinth

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

2,412件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello aravinthkumar,

     For image of android71.1.2 , 4gb is not enough, please use 8GB eMMC.

Have a nice day!

TIC weidong

0 件の賞賛
返信

2,412件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi weidong.sun‌,

I have tried with 8GB sd card. It's booting but it get stuck after few seconds.

Args:

Kernel command line: console=ttymxc0,115200 init=/init video=mxcfb0:off video=mxcfb1:off video=mxcfb2:off vido=mxcfb3:off vmalloc=256M androidboot.console=ttymxc0 consoleb
lank=0 androidboot.hardware=freescale cma=384M androidboot.selinux=disabled androidboot.dm_verity=disabled androidboot.serialno=1b2429d4ea997115 androidboot.storage_type=e
mmc

Bootlog:

EXT4-fs (mmcblk1p3): mounted filesystem with ordered data mode. Opts: barrier=1
EXT4-fs (mmcblk1p10): Ignoring removed nomblk_io_submit option
EXT4-fs (mmcblk1p10): 1 truncate cleaned up
EXT4-fs (mmcblk1p10): recovery complete
EXT4-fs (mmcblk1p10): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic
EXT4-fs (mmcblk1p4): Ignoring removed nomblk_io_submit option                                                          
EXT4-fs (mmcblk1p4): recovery complete                                                                                 
EXT4-fs (mmcblk1p4): mounted filesystem with ordered data mode. Opts: nomblk_io_submit                                 
EXT4-fs (mmcblk1p5): mounted filesystem with ordered data mode. Opts: (null)                                           
file system registered                                                                                                 
using random self ethernet address                                                                                     
using random host ethernet address                                                                                     
zram0: detected capacity change from 0 to 314572800                                                                    
logd.auditd: start                                                                                                     
logd.klogd: 8102597334                                                                                                 
Adding 307196k swap on /dev/block/zram0.  Priority:-1 extents:1 across:307196k SS                                      
binder: 260:260 transaction failed 29189, size 0-0                                                                     
logd.daemon: reinit                                                                                                    
sabresd_6dq:/ # healthd: No battery devices found                                                                      
ERROR: v4l2 capture: slave not found! V4L2_CID_HUE                                                                     
ERROR: v4l2 capture: slave not found! V4L2_CID_HUE                                                                     
init: Service 'surfaceflinger' (pid 264) killed by signal 11                                                           
init: Service 'surfaceflinger' (pid 264) killing any children in process group                                         
init: Service 'zygote' is being killed...                                                                              
init: Service 'zygote' (pid 269) killed by signal 9
init: Service 'zygote' (pid 269) killing any children in process group
init: write_file: Unable to open '/sys/android_power/request_state': No such file or directory
init: write_file: Unable to write to '/sys/power/state': Invalid argument
init: Service 'audioserver' is being killed...
init: Service 'cameraserver' is being killed...
init: Service 'media' is being killed...

sabresd_6dq:/ #
sabresd_6dq:/ # ERROR: v4l2 capture: slave not found! V4L2_CID_HUE
ERROR: v4l2 capture: slave not found! V4L2_CID_HUE

sabresd_6dq:/ # init: Starting service 'zygote'...
init: Starting service 'audioserver'...
init: Starting service 'cameraserver'...
init: Starting service 'media'...
init: couldn't write 428 to /dev/cpuset/camera-daemon/tasks: No such file or directory
init: Starting service 'netd'...
init: Starting service 'surfaceflinger'...

*************************** Get Stuck **********************************

Can you help on this.!

Regards,

Aravinth

0 件の賞賛
返信

2,412件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi weidong.sun‌,

I will try on 8GB card and it have any issue i will come back with this soon.

From which version of android we need a 8GB card.?

Update:

I found below line in your Android User Guide Document.

The minimum size of the SD card is 4 GB.

Regards,

Aravinth

0 件の賞賛
返信