MCLK from GPIO_0 or any other GPIO.?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCLK from GPIO_0 or any other GPIO.?

ソリューションへジャンプ
1,220件の閲覧回数
prev
Contributor II

I want to generate MCLK for Audio Codec section.

From Sabre Evaluation board, CSI_MCLK is generated from GPIO_0,

My understanding is that CCM clock can be generated from the below pins of GPIO_0, GPIO_5, GPO_19.

Can we generate the same MCLK from any other GPIO ? or we need to use only these.

pastedImage_0.png

Please clarify me

Thanks

M. Prev Ravanth

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,024件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Prev

no, from any other GPIOs it is not possible to generate clock.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,025件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Prev

no, from any other GPIOs it is not possible to generate clock.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,024件の閲覧回数
prev
Contributor II

Hi Igor,

Can i use  NANDF_CS2 for clock generation of Audio MCLK

pastedImage_0.png

Thanks

M. Prev Ravanth

0 件の賞賛
返信