According the BSDL file MCIMX6U7CVM08 is the boundary scan register length 648 bits, is this correct??
I am having a lot of problems when I am using this device in an interconnect test (Jtag Technologies soft/hardware).
Device id test is passing.
Kind regards, Hans
Original Attachment has been moved to: MX6S_TO1.1.bsdl.zip
已解决! 转到解答。
Hello,
Below are some general considerations.
1.
Please check if PCIe voltages are applied :
according to footnote of Table 2-21 (Recommended connections for unused
analog interfaces) of the Hardware Development Guide, linked below ,
SATA and PCIe supplies must remain powered if boundary scan test needs to be done.
< http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf >
2.
JTAG_MOD (SJC_MOD) should be pulled up (to NVCC_JTAG) for Boundary Scan Mode.
3.
Please check in BSDL file is correct for the i.MX6 part.
Please use the recent BSDL file from the Freescale Web :
“MX6DL_TO1.1.bsdl” file for i.MX6 DL.
Note :
“attribute BOUNDARY_LENGTH of MX6DL: entity is 648;”
4.
Please pay attention on COMPLIANCE_PATTERNS of the BSDL file.
attribute COMPLIANCE_PATTERNS of MX6S: entity is
"(TEST_MODE, JTAG_MOD, POR_B) (011)";
Check if :
TEST_MODE is LOW ;
JTAG_MOD is HIGH ;
POR_B is HIGH.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
Below are some general considerations.
1.
Please check if PCIe voltages are applied :
according to footnote of Table 2-21 (Recommended connections for unused
analog interfaces) of the Hardware Development Guide, linked below ,
SATA and PCIe supplies must remain powered if boundary scan test needs to be done.
< http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf >
2.
JTAG_MOD (SJC_MOD) should be pulled up (to NVCC_JTAG) for Boundary Scan Mode.
3.
Please check in BSDL file is correct for the i.MX6 part.
Please use the recent BSDL file from the Freescale Web :
“MX6DL_TO1.1.bsdl” file for i.MX6 DL.
Note :
“attribute BOUNDARY_LENGTH of MX6DL: entity is 648;”
4.
Please pay attention on COMPLIANCE_PATTERNS of the BSDL file.
attribute COMPLIANCE_PATTERNS of MX6S: entity is
"(TEST_MODE, JTAG_MOD, POR_B) (011)";
Check if :
TEST_MODE is LOW ;
JTAG_MOD is HIGH ;
POR_B is HIGH.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks Yuri,
I find out yesterday that the PCIE voltage is connected to GND , so I think I can stop debugging!
Only the device_id is read out correct.
Thanks, Hans
Met vriendelijke groet,
Kind regards/mit freundlichen Grüßen,
tbp electronics bv
Hans Hogendoorn
test design engineer
E hhogendoorn@tbp.nl<mailto:hhogendoorn@tbp.nl>
T +31187602744
@tbp: Monday to Friday
Van: Yuri
Verzonden: donderdag 19 november 2015 7:11
Aan: Hans Hogendoorn
Onderwerp: Re: - MCIMX6U7CVM08 BSDL
<http://jiveon.jivesoftware.com/mpss/c/8gA/PDcDAA/t.1s9/Wajh6HUHRUScEqDJ-BXGwQ/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQ-3D>
MCIMX6U7CVM08 BSDL
reply from Yuri Muhin<http://jiveon.jivesoftware.com/mpss/c/8gA/PDcDAA/t.1s9/Wajh6HUHRUScEqDJ-BXGwQ/h1/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQuFPEPvxbIEdmXkTIJKJlvLtE60ovg1JsmwU97EV8kDnyQobvus7WCo5HCX-2B1MKb0-3D> in i.MX Community - View the full discussion<http://jiveon.jivesoftware.com/mpss/c/8gA/PDcDAA/t.1s9/Wajh6HUHRUScEqDJ-BXGwQ/h2/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bSOyR7kSuD7b-2FWroe3nZSfEUvWD4L-2BqOiWoHFWedvjONlgHUQ5dEt-2FrUd6I-2BiMxrEA-3D>