LPSPI2 on i.MX 8ULP - A35 vs M33

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPSPI2 on i.MX 8ULP - A35 vs M33

824件の閲覧回数
ericnelsonaz
Contributor III

Is it possible to move the LPSPI2 peripheral on the i.MX 8ULP from the default Cortex M33 to the Cortex A35?

ラベル(1)
タグ(1)
0 件の賞賛
返信
5 返答(返信)

674件の閲覧回数
ericnelsonaz
Contributor III

I believe that my original question was off-base because the LPSPI2 port and other peripherals connected through PBRIDGE2 don't appear to be available to either the M33 or A35. They appear to be accessible only on the DSP.

Can someone confirm this or let me know how we can access the PBRIDGE2 peripherals (LPI2C2/3, LPSPI2/3, and LPUART2/3) on either or both the A35 and M33?

350件の閲覧回数
martinetd
Contributor IV

hi @ericnelsonaz 

Have you been able to access LPSPI2 from anywhere (m33 or a35) after this?

FWIW I've tried and reached the same conclusion wrt the DSP domain; LPSPI2 is on PBRIDGE2 and I couldn't manage to make the m33 core access it. I've asked about it here last week (no reply at this point, but it's been less than a week): https://community.nxp.com/t5/i-MX-Processors/i-MX8ULP-access-pbridge2-from-m33/td-p/1923507

As a workaround I'm trying spi-gpio with gpio forwarded over the m33 core, but it'd be great if there could be a way to use the pbridge2 peripherals that are just unused otherwise...

0 件の賞賛
返信

345件の閲覧回数
ericnelsonaz
Contributor III

No. We didn't find a solution.

We used spi-gpio as a stopgap and then reworked out board.

0 件の賞賛
返信

807件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Sorry for the i.MX8ULP is still on Preproduction, we can not give proper support for it.You can try to connect the dfae you buy the product from, they will support. Sorry about it

0 件の賞賛
返信

688件の閲覧回数
ericnelsonaz
Contributor III

Hi @Rita_Wang 

Is it possible to get some more information on this now that the i.MX 8ULP has been released?