LOCSC Interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LOCSC Interface

3,033件の閲覧回数
rubensjunior
Contributor IV

Dear collegues! Happy 2020!

Does anyone know of an interface called locsc for NXP processors?

Best regards.

Rubens Júnior.

3 返答(返信)

2,911件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Rubens

I never heard that such interface was used with i.mx processors, could you provide

some additional info or links about that interface.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,911件の閲覧回数
rubensjunior
Contributor IV

Hi igorpadykov,

The LOCSC is a CMOS interface (No NXP).

I need to migrate a project that uses a LOCSC to CMOS Sensor Interface (CIS) using the iMXRT1051 processor. How I do?

Best Regards,

Rubens Júnior

0 件の賞賛
返信

2,911件の閲覧回数
igorpadykov
NXP Employee
NXP Employee