LCD Linux driver for N101ICG-L21 TFT Liquid Crystal Display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LCD Linux driver for N101ICG-L21 TFT Liquid Crystal Display

791 Views
ayanavincent
Contributor I

N101ICG-L21 is a 10" (10.1" diagonal) TFT Liquid Crystal Display module with LED
Backlight unit and 40 pins LVDS interface. This module supports 1280 x 800 WXGA mode.

For i.mx6 Quad board I'm using Yocto Daisy SDK version 1.6.

Hannstar LCD is using "egalax " Linux driver.

Please help me to find out the Linux driver for N101ICG-L21

Labels (1)
0 Kudos
Reply
1 Reply

606 Views
igorpadykov
NXP Employee
NXP Employee

Hi ayana

you can check lcds with similar resolutions if these will work for you

Re: IMX53 with lvds 1280x800 resolution

http://boundarydevices.com/1280x800-displays/

http://boundarydevices.com/i-mx6-kernel-l3-0-35_4-0-0/

LCD driver customization is decribed in

Chapter 18 "Supporting the i.MX53 Reference Board DISP0 LCD"

MX53UG

Best regards

igor

0 Kudos
Reply