N101ICG-L21 is a 10" (10.1" diagonal) TFT Liquid Crystal Display module with LED
Backlight unit and 40 pins LVDS interface. This module supports 1280 x 800 WXGA mode.
For i.mx6 Quad board I'm using Yocto Daisy SDK version 1.6.
Hannstar LCD is using "egalax " Linux driver.
Please help me to find out the Linux driver for N101ICG-L21
Hi ayana
you can check lcds with similar resolutions if these will work for you
Re: IMX53 with lvds 1280x800 resolution
http://boundarydevices.com/1280x800-displays/
http://boundarydevices.com/i-mx6-kernel-l3-0-35_4-0-0/
LCD driver customization is decribed in
Chapter 18 "Supporting the i.MX53 Reference Board DISP0 LCD"
Best regards
igor