Hi
we planned to use imx6UL series processor for our project( partnumber : MCIMX6G3CVM05AB) we were referring to KIT6UL-3001EVM for reference schematics same attached for reference.
As per page number 10 in the attached schematics The signal name DRAM_1V35 is shorted with GND of PMIC(U713- Pin 24) please Clarify why.
There is a connection to NC2(pin-23) and NC3(pin-25) of U713 also. where datasheet says it is No connection. Please clarify.
https://freescale.jiveon.com/docs/DOC-331899
@shivakumar1
Hello,
The connections, You mentioned, are correct for PMIC PF3000.
This is one of differences between PF3000 and PF3001: PF3000
supports VREFDDR generation, bit PF3001 - does not.
Regards,
Yuri.