KIT6UL-3001EVM Clarification required

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KIT6UL-3001EVM Clarification required

429 Views
shivakumar1
Contributor II

Hi

we planned to use imx6UL series processor for our project( partnumber : MCIMX6G3CVM05AB)  we were referring to KIT6UL-3001EVM for reference schematics same attached for reference.

As per page number 10 in the attached schematics The signal name DRAM_1V35 is shorted with GND of PMIC(U713- Pin 24) please Clarify why. 

There is a connection to NC2(pin-23) and NC3(pin-25) of U713 also. where datasheet says it is No connection. Please clarify.

 

https://freescale.jiveon.com/docs/DOC-331899

 

shivakumar1_0-1605592135962.png

 

0 Kudos
1 Reply

426 Views
Yuri
NXP Employee
NXP Employee

@shivakumar1 
Hello,

  The connections, You mentioned, are correct for PMIC PF3000.
This is one of differences between PF3000 and PF3001: PF3000
supports VREFDDR generation, bit PF3001 - does not.

 

Regards,
Yuri.

0 Kudos