I'm tryng to download a Linux image to my iMX93-QSB using UUU in Windows 10. First of all, i installed LF_v6.6.3-1.0.0_images_IMX93EVK from https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for... , then i unzipped it into a folder on Desktop. Then i installed the latest version of uuu.exe from https://github.com/nxp-imx/mfgtools/releases ,placing it in the same folder as the images together with libusb-1.0.dll.
Eventually, I did the following steps:
1. set the boot mode on "Serial Download".
2. turned on the board.
3. I opened cmd as administrator, and wrote:
In this way, I checked USB connection.
4. I used this command in order to start the download:
I can't figure out what's wrong. Can you help me?
Is imx-boot-imx93-9x9-lpddr4-qsb-sd.bin-flash_singleboot the file that contains SPL, U-BOOT, etc.. and correctly compiled for iMX93-QSB Evaluation board?
If not, which one can I use? Should I compile SPL and U-BOOT by myself?
Regards,
Roberto.
Hi @Bob_NXP_user!
Thank you for contacting NXP Support!
Can you open Powershell in administrator mode?
Also, can you try with the command "uuu.exe uuu.auto-imx93-9x9-lpddr4-qsb"
The option emmc_all is to write uboot and rootfs can you try too with "uuu.exe -b emmc imx-boot-imx93-9x9-lpddr4-qsb-sd.bin-flash_singleboot"
Best Regards!
Chavira
Hi @Chavira, Thanks for replying!
I solved this issue by changing USB drivers and removing my USB hub.
Now I'm able to access the bootloader from serial port, I would like to ask you another question. How can i download dtb and kernel on my board?
I checked into LF_v6.6.3-1.0.0_images_IMX93EVK folder and i found imx93-9x9-qsb.dtb, i think that's the file i need but I don't know how to download it. Then I was also looking for the kernel file in the same folder but I didn't find it, maybe I just can't recognize it, can you help me?
Hi @Bob_NXP_user
I am also facing the same issue!
Please tell me the steps you took to resolve the issue.
It will be helpful.
Thanks
Shubham
Hi
Actually, I am trying to flash the imx93 board as :
./uuu -b emmc_all imx-boot-imx93-11x11-lpddr4x-evk-sd.bin-flash_singleboot imx-image-full-imx93-11x11-lpddr4x-evk-20240829072649.rootfs.wic.zst/*
but I am also getting this error :
LIBUSB TIMEOUT ERROR as exactly like you have posted.
You said yos resolved by updating some USB drivers or anything. Please tell me how can I also resolve this issue?
Thanks
Actually, I am working on linux any idea how to resolve this in linux system?