Hi All,
I am trying to flash Android Auto (Android P9.0.0_1.0.2_AUTO_Alpha) prebuilt image to IMX8qxp MEK board using UUU tool. UUU tool is failed to flash the image onto the reference board at ERASE userdata. The steps executed as per the Android Quick start guide document.
I have modified partition table data in the uuu script (uuu-android-mx8qxp-mek-emmc.lst) as the EMMC size is 32GB.
This is the last message shown while executing the uuu tool
Success 0 Failure 0
1/ 0 [ ]
1:3 19/21 [============100%============] FB[-t 600000]: ERASE userdata
After uuu tool stops
Success 0 Failure 0
1/ 0 [ ]
Success 0 Failure 0
Success 0 Failure 1
1/ 0 [ ]
I have attached the console log along with this. Please help me on this.
The partition table change made issue in flashing. The default uuu-android-mx8qxp-mek-emmc.lst script worked without any change.
HI Joan Xie,
We could able to flash and boot the iMX8qxp MEK board with uuu-android-mx8qxp-mek-emmc.lst script. But in storage the size is showing as 16GB instead of 32GB( this is the actual size of Emmc in MEK board). The image is attached along with this reply for reference. I guess we need to change the partition image to get 32GB of storage, but when we change the partition image name to "partition-table-29GB.img" then flashing steps is getting failed.
Hi joan,
yes it was an TYPO. We replaced to "partition-table-28GB.img" in the uuu script.