i.MX6 HDMI L-PCM support.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 HDMI L-PCM support.

Jump to solution
924 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6SDL HDMI.

I have understood i.MX6DL HDMI support 16, 24 bits L-PCM in https://community.freescale.com/thread/349086.

Then, please see chapter 13.2.5 in IMX6SDLLXRM Rev.Rev L3.0.35_4.1.0 (for L3.0.35_4.1.0_BSP).

24 bits audio is not mentioned in this chapter.

In addition, in sound/soc/imx/imx-hdmi-dma.c in L3.0.35_4.1.0, there is the following comment.

/* 24bit not support now. */

So we understood i.MX6SDL supports 24 bits L-PCM, but driver is not supported.

Is this correct?

Best Regards,

Satoshi Shimoda

Labels (5)
Tags (2)
0 Kudos
Reply
1 Solution
654 Views
joanxie
NXP TechSupport
NXP TechSupport

mx6 can support 24bits, different bsp version has different driver support. normally you can configure the asound.conf to support it.

View solution in original post

0 Kudos
Reply
2 Replies
654 Views
eric_kang
Contributor II

Dear All,

I have a same problem in the customer board.

I'm using the i.MX6Q / Linux 3.14.52

Could you tell me how to confirm the 24bit HDMI Audio on i.MX6 Evaluation board?

Best Regards,

Eric.

0 Kudos
Reply
655 Views
joanxie
NXP TechSupport
NXP TechSupport

mx6 can support 24bits, different bsp version has different driver support. normally you can configure the asound.conf to support it.

0 Kudos
Reply