Issue in Video Streaming with gadget webcam module g_webcam in i.MX8 EVK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issue in Video Streaming with gadget webcam module g_webcam in i.MX8 EVK

4,359 次查看
sunithas
Contributor I

Issue:
Not able to stream video in VLC from the sample mjpg file using gadget webcam module.
DWC3 controller stops submitting the USB Request back to the g_webcam module.

Followed below steps :

1.Download i.MX8 linux source 4.9.88
[git clone https://source.codeaurora.org/external/imx/linux-imx -b imx_4.9.88_2.0.0_ga]
2.Download UVC gadget test application [https://github.com/lintwins/uvc-gadget]

2. Enable g_webcam module in linux kernel configuration
Device Drivers > USB Support > USB Gadget Support > USB Webcam Function

3.Compilation
3.1. Cross-Compile i.MX8 source code
$ sudo apt-get install crossbuild-essential-arm64
$ make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu-
3.2. Update KERNEL_DIR, CROSS_COMPILE, ARCH in the UVC gadget test application Makefile
3.3. Cross-Compile UVC gadget application for i.MX8 platform
$ make

4. i.MX8 SD card preparation
4.1
4.1 Copy 'g_webcam.ko' and 'usb_f_uvc.ko' to /media/user/rootfs/home/root/
4.2. Copy 'uvc-gadget' executable /media/user/rootfs/home/root/
4.3. Copy sample mjpg file [640x360/1280x720] to /media/user/rootfs/home/root/

5. Insert SD card and power ON the i.MX8 platform

6. Execution
6.1. Load gadget webcam modules
$ insmod usb_f_uvc.ko
$ insmod g_webcam.ko streaming_maxpacket=1024
6.2. Run uvc gadget test application
$ ./uvc-gadget -d /dev/videoX -i <sample-mjpg-file-name>
ex: $ ./uvc-gadget -d /dev/video1 -i 1280x720.mjpg (or)
$ ./uvc-gadget -d /dev/video1 -i 640x360.mjpg
Run VLC on the streaming linux PC and start the stream with the corresponding resolution 1280x720 (or) 640x360

Please suggest if I have missed anything or where I am going wrong.

Thanks,

Sunitha

标记 (2)
0 项奖励
回复
2 回复数

3,049 次查看
art
NXP Employee
NXP Employee

Does your host PC ever detect the i.MX8 hardware as the UVC device? Please check.

0 项奖励
回复

3,049 次查看
sunithas
Contributor I

Hi Arthur,

Yes. Host PC detected i.MX8 Hardware as UVC device.

When we start streaming video data, gadget controller driver stopped submitting usb request to the gadget driver

Regards,

Sunitha

0 项奖励
回复