Is it possible to do QuadSPI NAND flash with the IMX6ULL?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to do QuadSPI NAND flash with the IMX6ULL?

ソリューションへジャンプ
1,828件の閲覧回数
djregan
Contributor III

Hello,  Per the NXP support page for the IMX6ULL...

i.MX 6ULL Applications Processor | Arm Cortex-A7|NXP 

...the IMX6ULL can support two channels of QSPI Nor Flash. But, is anyone aware of whether or not folks have also been able to leverage QSPI NAND flash with the IMX6ULL?

If 'Yes.'... is there an app note / article / white paper that discusses the effort?

Thanks much in advance!

--DJ Regan

imx6ul

qspi-nor‌

#qspi-nand

QuadSPI‌

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,095件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Regan

QSPI was designed to work with QSPI NOR and was not tested with NAND. Seems there may be problems

due to differencies with timings and data structures.

>Would it be possible (in theory) to connect a QSPI NOR flash to QSPI-A, and a QSPI NAND flash to QSPI-B?

I am afraid not

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,095件の閲覧回数
djregan
Contributor III

Hi Igor,

Understood. We'll make plans accordingly.

Appreciate it sir!

--DJ

0 件の賞賛
返信
1,095件の閲覧回数
djregan
Contributor III

Expanding on the above question...

Would it be possible (in theory) to connect a QSPI NOR flash to QSPI-A, and a QSPI NAND flash to QSPI-B?

The idea would then be...

The QSPI NOR flash provides boot-up support while the QSPI NAND flash provides file system support.

--DJ Regan

0 件の賞賛
返信
1,096件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Regan

QSPI was designed to work with QSPI NOR and was not tested with NAND. Seems there may be problems

due to differencies with timings and data structures.

>Would it be possible (in theory) to connect a QSPI NOR flash to QSPI-A, and a QSPI NAND flash to QSPI-B?

I am afraid not

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信