Is it possible to do QuadSPI NAND flash with the IMX6ULL?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to do QuadSPI NAND flash with the IMX6ULL?

Jump to solution
1,757 Views
djregan
Contributor III

Hello,  Per the NXP support page for the IMX6ULL...

i.MX 6ULL Applications Processor | Arm Cortex-A7|NXP 

...the IMX6ULL can support two channels of QSPI Nor Flash. But, is anyone aware of whether or not folks have also been able to leverage QSPI NAND flash with the IMX6ULL?

If 'Yes.'... is there an app note / article / white paper that discusses the effort?

Thanks much in advance!

--DJ Regan

imx6ul

qspi-nor‌

#qspi-nand

QuadSPI‌

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
1,024 Views
igorpadykov
NXP Employee
NXP Employee

Hi Regan

QSPI was designed to work with QSPI NOR and was not tested with NAND. Seems there may be problems

due to differencies with timings and data structures.

>Would it be possible (in theory) to connect a QSPI NOR flash to QSPI-A, and a QSPI NAND flash to QSPI-B?

I am afraid not

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
1,024 Views
djregan
Contributor III

Hi Igor,

Understood. We'll make plans accordingly.

Appreciate it sir!

--DJ

0 Kudos
Reply
1,024 Views
djregan
Contributor III

Expanding on the above question...

Would it be possible (in theory) to connect a QSPI NOR flash to QSPI-A, and a QSPI NAND flash to QSPI-B?

The idea would then be...

The QSPI NOR flash provides boot-up support while the QSPI NAND flash provides file system support.

--DJ Regan

0 Kudos
Reply
1,025 Views
igorpadykov
NXP Employee
NXP Employee

Hi Regan

QSPI was designed to work with QSPI NOR and was not tested with NAND. Seems there may be problems

due to differencies with timings and data structures.

>Would it be possible (in theory) to connect a QSPI NOR flash to QSPI-A, and a QSPI NAND flash to QSPI-B?

I am afraid not

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply