Interfacing BT HCI to iMX6 UART

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Interfacing BT HCI to iMX6 UART

跳至解决方案
1,259 次查看
mohammedazlum
Contributor IV

Hello,

I have a Bluetooth module with HCI UART interface (HCI_TX, HCI_RX, HCI_CTS, HCI_RTS). I would like to know that, can I interface this HCI BT module directly with iMX6 UART port ?

Or do we need to put any bridge between HCI BT and iMX6 CPU for interface compatibility ?

Regards,

Azlum

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,022 次查看
igorpadykov
NXP Employee
NXP Employee

Hi mohammed

yes it can be connected directly, one needs just to check signal levels.

HCI provides a uniform messaging protocol, which allows application software

from one vendor to be used with a Bluetooth from another vendor.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,022 次查看
mohammedazlum
Contributor IV

Thanks Igor.

I will take care logic levels while interfacing !.

Regards,

Azlum

0 项奖励
回复
1,023 次查看
igorpadykov
NXP Employee
NXP Employee

Hi mohammed

yes it can be connected directly, one needs just to check signal levels.

HCI provides a uniform messaging protocol, which allows application software

from one vendor to be used with a Bluetooth from another vendor.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复