Interfacing BT HCI to iMX6 UART

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interfacing BT HCI to iMX6 UART

ソリューションへジャンプ
1,866件の閲覧回数
mohammedazlum
Contributor IV

Hello,

I have a Bluetooth module with HCI UART interface (HCI_TX, HCI_RX, HCI_CTS, HCI_RTS). I would like to know that, can I interface this HCI BT module directly with iMX6 UART port ?

Or do we need to put any bridge between HCI BT and iMX6 CPU for interface compatibility ?

Regards,

Azlum

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,629件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi mohammed

yes it can be connected directly, one needs just to check signal levels.

HCI provides a uniform messaging protocol, which allows application software

from one vendor to be used with a Bluetooth from another vendor.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,629件の閲覧回数
mohammedazlum
Contributor IV

Thanks Igor.

I will take care logic levels while interfacing !.

Regards,

Azlum

0 件の賞賛
返信
1,630件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi mohammed

yes it can be connected directly, one needs just to check signal levels.

HCI provides a uniform messaging protocol, which allows application software

from one vendor to be used with a Bluetooth from another vendor.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信