Information on the L2 Cache Controller for the I.MX6 ULL?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Information on the L2 Cache Controller for the I.MX6 ULL?

524 次查看
robertstewart
Contributor I

Hi,

I'm doing bare metal coding on an SOC containing an I.MX6 ULL. I've going through the NXP Applications Processor Reference Manual for this processor and can find no details on the L2 cache controller, like its mmio address or the controller name. Is it a PL310 controller similar to an A9 processor?

Thanks for any insight you can give me.

Bob

标签 (1)
标记 (3)
2 回复数

375 次查看
ko-hey
Senior Contributor II

Does someone have information for this question ?

I have same question.

Ko-hey

#i.mx6ull#l2 cache#pl310

0 项奖励

375 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  I.MX 6ULL does not have separate L2 cache controller / module.
L2  is just part of core.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------