Information on the L2 Cache Controller for the I.MX6 ULL?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Information on the L2 Cache Controller for the I.MX6 ULL?

512 Views
robertstewart
Contributor I

Hi,

I'm doing bare metal coding on an SOC containing an I.MX6 ULL. I've going through the NXP Applications Processor Reference Manual for this processor and can find no details on the L2 cache controller, like its mmio address or the controller name. Is it a PL310 controller similar to an A9 processor?

Thanks for any insight you can give me.

Bob

Labels (1)
Tags (3)
2 Replies

363 Views
ko-hey
Senior Contributor II

Does someone have information for this question ?

I have same question.

Ko-hey

#i.mx6ull#l2 cache#pl310

0 Kudos

363 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I.MX 6ULL does not have separate L2 cache controller / module.
L2  is just part of core.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------