Inflexion demo hangs at IFXF_Initialize function.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Inflexion demo hangs at IFXF_Initialize function.

1,088件の閲覧回数
SharanK
Contributor II

Hi,

I have built the inflexion demo in the Linux environment.

After the successful build,  I run the exe on a target, but the problem is the exe runs till I get a print

"Running on IMX 53" and then it hangs.

The problem is most probably is happening in engine config part of IFXF_Initialize function in framework_linux_generic.c. But i am unable proceed further.

Please help.

Thanks in advance,

Sharan K

タグ(2)
0 件の賞賛
返信
0 返答(返信)