Hi sir:
I play two different 1080P video and two different devices output at the same time.
Boot command:
setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk1p1 init=/init rootwait video=mxcfb0:dev=hdmi,1920x1080M@60,
if=RGB24 video=mxcfb1:dev=lcd,LCD-1920x1080,if=RGB24 dmfc=3'
Play 1080P high quality video by gst-launch video by
gst-launch playbin2 uri=file:////mnt/disk/Girl1.avi video-sink="mfw_v4lsink device=/dev/video16" audio-sink="alsasink device=plughw:0" &
gst-launch playbin2 uri=file:////mnt/disk/snsd.mp4 video-sink="mfw_v4lsink device=/dev/video18" audio-sink="alsasink device=plughw:1" &
I can see color bar at top of screen as attach files.
I play low quality file and it's works fine.
Is it i.mx6Q limitation ?
解決済! 解決策の投稿を見る。
The video16 is for GUI, so if you put the video on it also, there will be some artifacts since there are 2 sources (GUI and video) updating the frame buffer.
For dual display mode, you should not use "dmfc=3", "dmfc=3" means all DMFC fifo will be used for DP, the main display. It should be used for only single display mode.
The strange color bar still exist when not use "dmfc=3.
Thanks!
Were you able to figure out the problem? I am having similar issues.
Thanks
Tim
Hi,
that is not the expected behaviour. Can you try this pipeline:
gst-launch -v videotestsrc ! 'video/x-raw-yuv, format=(fourcc)NV12, width=(int)1920, height=(int)1080, framerate=(fraction)10/1' ! mfw_v4lsink
Do you see the bar in this case?
Hi,
I had tried this solution.
It worked fine. Strange color bar did not exist.
In addition, I found that the display was normal if frame buffer console option was disabled.
And video16 change to video17 can work fine.
It's framebuffer issue?
The video16 is for GUI, so if you put the video on it also, there will be some artifacts since there are 2 sources (GUI and video) updating the frame buffer.
You mean the video must setting to 17 if used dual-display. But not have any document explain it.
Have you tried with Android?
What are the steps to test for dual display on android?
I have tried but not find any solution for this..
I only tried to test on Linux base.
Thanks!