Imx6 yocto how to integrerate the kernel module with core image base

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Imx6 yocto how to integrerate the kernel module with core image base

1,253件の閲覧回数
bala955
Contributor I

Hi Team

I am trying to integrate the lm75 driver kernel module in core base image for imx6ull EVK.

The BSP version is 2023.04-r0

I keep the driver source inside the following folder location

 

Iam getting the following error when building the bitbake lm75-mod

 

Following changes i did in local.conf

Screenshot from 2024-01-17 12-12-35.pngScreenshot from 2024-01-17 12-16-01.pngScreenshot from 2024-01-17 12-17-45.png

 

Please help me to fix the issue ASAP

 

0 件の賞賛
返信
3 返答(返信)

1,224件の閲覧回数
bala955
Contributor I

thank you for the information

I have another doubt where can I make a change to downgrade the kernel version from 6.1 to 5. or 4.

in yocto source ?

Please reply

0 件の賞賛
返信

1,223件の閲覧回数
bala955
Contributor I

pleas tell which file to modify to do kernel migration changes and next steps to be done in yocot for imx6

0 件の賞賛
返信