Imx53 can't boot from nandflash K9F4G08UOB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Imx53 can't boot from nandflash K9F4G08UOB

ソリューションへジャンプ
1,971件の閲覧回数
cherncharley
Contributor I

I can't boot imx53 from nandflash K9F4G08UOB. My config gpio is :

NAND Boot  Descriptions

BOOT_CFG1[7] -------------1 - Boot from Nand Interface

BOOT_CFG1[6] -------------1 - EIM Pads

BOOT_CFG1[5:4]-----------00 - No Interleaving

BOOT_CFG1[3:2]-----------10 - 5 Address Cycles

BOOT_CFG2[7:6] ----------01 - 2KB + 64 Bytes (4-bit ECC)

BOOT_CFG2[5]--------------0 - 8 bit

BOOT_CFG2[2]--------------0 - AXI DDR divide by 12

BOOT_CFG3[7]--------------1 - 8 Blocks, Stride Size (Bad Block skip step)

BOOT_CFG3[6]--------------0 - Non LBA (11ms delay)

BOOT_CFG3[5]--------------1 - Yes NAND Use R/B Signals

BOOT_CFG3[4:3]-----------00 - 4-bit ECC Page Size=00/01/10 

BOOT_CFG3[2:1]-----------01 64 Pages In Block

 

And

BT_FREQ--------------0

BT_MMU_ENABLE---------------1

AXI/DDR Fre -----------------1

OSC_Freq_SE-------------1

 

Is there any one can help me look at this config is ok for K9F4G08UOB ?

Thank you!

Original Attachment has been moved to: ucl.xml.zip

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 解決策
1,559件の閲覧回数
cherncharley
Contributor I

I have work out. It is because the size of uboot.bin too large.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,560件の閲覧回数
cherncharley
Contributor I

I have work out. It is because the size of uboot.bin too large.

0 件の賞賛
返信
1,559件の閲覧回数
VladanJovanovic
NXP Employee
NXP Employee

It would help if you would provide entire output from serial console that you get when you try to run MfgTool with the above ucl.xml setup.

0 件の賞賛
返信