Imx53 can't boot from nandflash K9F4G08UOB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx53 can't boot from nandflash K9F4G08UOB

Jump to solution
1,815 Views
cherncharley
Contributor I

I can't boot imx53 from nandflash K9F4G08UOB. My config gpio is :

NAND Boot  Descriptions

BOOT_CFG1[7] -------------1 - Boot from Nand Interface

BOOT_CFG1[6] -------------1 - EIM Pads

BOOT_CFG1[5:4]-----------00 - No Interleaving

BOOT_CFG1[3:2]-----------10 - 5 Address Cycles

BOOT_CFG2[7:6] ----------01 - 2KB + 64 Bytes (4-bit ECC)

BOOT_CFG2[5]--------------0 - 8 bit

BOOT_CFG2[2]--------------0 - AXI DDR divide by 12

BOOT_CFG3[7]--------------1 - 8 Blocks, Stride Size (Bad Block skip step)

BOOT_CFG3[6]--------------0 - Non LBA (11ms delay)

BOOT_CFG3[5]--------------1 - Yes NAND Use R/B Signals

BOOT_CFG3[4:3]-----------00 - 4-bit ECC Page Size=00/01/10 

BOOT_CFG3[2:1]-----------01 64 Pages In Block

 

And

BT_FREQ--------------0

BT_MMU_ENABLE---------------1

AXI/DDR Fre -----------------1

OSC_Freq_SE-------------1

 

Is there any one can help me look at this config is ok for K9F4G08UOB ?

Thank you!

Original Attachment has been moved to: ucl.xml.zip

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
1,403 Views
cherncharley
Contributor I

I have work out. It is because the size of uboot.bin too large.

View solution in original post

0 Kudos
Reply
2 Replies
1,404 Views
cherncharley
Contributor I

I have work out. It is because the size of uboot.bin too large.

0 Kudos
Reply
1,403 Views
VladanJovanovic
NXP Employee
NXP Employee

It would help if you would provide entire output from serial console that you get when you try to run MfgTool with the above ucl.xml setup.

0 Kudos
Reply