I can't boot imx53 from nandflash K9F4G08UOB. My config gpio is :
NAND Boot Descriptions
BOOT_CFG1[7] -------------1 - Boot from Nand Interface
BOOT_CFG1[6] -------------1 - EIM Pads
BOOT_CFG1[5:4]-----------00 - No Interleaving
BOOT_CFG1[3:2]-----------10 - 5 Address Cycles
BOOT_CFG2[7:6] ----------01 - 2KB + 64 Bytes (4-bit ECC)
BOOT_CFG2[5]--------------0 - 8 bit
BOOT_CFG2[2]--------------0 - AXI DDR divide by 12
BOOT_CFG3[7]--------------1 - 8 Blocks, Stride Size (Bad Block skip step)
BOOT_CFG3[6]--------------0 - Non LBA (11ms delay)
BOOT_CFG3[5]--------------1 - Yes NAND Use R/B Signals
BOOT_CFG3[4:3]-----------00 - 4-bit ECC Page Size=00/01/10
BOOT_CFG3[2:1]-----------01 64 Pages In Block
And
BT_FREQ--------------0
BT_MMU_ENABLE---------------1
AXI/DDR Fre -----------------1
OSC_Freq_SE-------------1
Is there any one can help me look at this config is ok for K9F4G08UOB ?
Thank you!
Original Attachment has been moved to: ucl.xml.zip
已解决! 转到解答。