Hi,
We are using RT1170 MCU for our cluster application.
When we are connecting 7" LCD to our custom board out of 7 boards we are getting unknown errors as attached screenshot in 3 boards(while we are running the code, its going to 'usagefault handler' after some time, the time is not definite)and CPU frequency stops and it is in hanging condition.Without connecting LCD everything works just fine.
Attached is the MCU ,SDRAM and LCD Schematics for your reference.
Let us know what possibly causing this issue?
已解决! 转到解答。
Hi @Kan_Li
We resolved issue .
As per recommendation FlexSPI_DQS pin should be left floating for 133Mhz.in our custom board we connected FlexSPI_DQS pin to GPIO function.
We reduced speed to 60Mhz now all the devices are working fine.
Thank you for your support
Thanks & Regards
Chethan B G
Hi @Chethanbg ,
If you have 7 custom boards, but 3 of them had this issue, I would suspect there might be some soldering issue on those boards, did rest of them behave normally as expected all the time? Please kindly clarify.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi @Chethanbg ,
Was the frame buffer for the LCD in a none cache area? If not, please do so and check if the problem is still there.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi @Kan_Li
We resolved issue .
As per recommendation FlexSPI_DQS pin should be left floating for 133Mhz.in our custom board we connected FlexSPI_DQS pin to GPIO function.
We reduced speed to 60Mhz now all the devices are working fine.
Thank you for your support
Thanks & Regards
Chethan B G